7EN02-0495-01

Meter status information

Two LEDs on the front panel indicate the current status of the device: the green status LED and the yellow energy pulsing LED.

The icons in the table below indicate the LED state:

  • = LED is off

  • = LED is on

  • = LED is flashing

Status LED

Energy pulsing LED

Description

Off

1 s >

On, no pulse counting

On, with pulse counting

Error, pulse counting stopped

Abnormal, with pulse counting

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?