Adding an EM3122 / EM3224 / EM3322 / EM3424 / EM3724 series meter to a site
- Start The ION Setup in Network mode.
- Right-click the site icon and select Insert Item.
- Select Device and then click OK. The New Device dialog appears.
- Enter a descriptive name for your device in the dialog box Name (for example, EM3224).
- Select PowerLogic EM3000 Series Energy Meter from the drop down list for the Type.
- Select Unit ID give the value between 1 to 247.
- Select the Group you want to assign
the device from the drop down list, and then click OK to go back to the Network Viewer.NOTE:
-
You may need to change the template option if the meter setup screens do not correctly reflect your meter Type.
- The Display tab dialog box will highlight the current Template Options when it has established communication with the meter. Select the appropriate Template Options (Default / METSEEM3122 / METSEEM3224 / METSEEM3322 / METSEEM3424 / METSEEM3724) for the device and then click OK to go back to the Network Viewer.
-