Configuration menu for EM3712
|
Section |
Parameter |
Options |
Description |
|---|---|---|---|
|
Wiring |
Type |
|
Select the power system type the meter is wired to. |
|
CT |
|
Define how many current transformers (CT) are connected to the meter and which terminals they are connected to. |
|
|
CT Ratio |
CT Secondary |
|
Select the size of the CT secondary, in Amps. |
|
CT Primary |
1 to 32767 |
Enter the size of the CT primary, in Amps. |
|
|
Frequency |
Frequency |
|
Select the frequency of the electrical power system, in Hz. |
|
Date |
Date |
DD-MMM-YYYY |
Set the current date using the specified format. |
|
Time |
Time |
hh:mm |
Set the time using the 24-hour format. |
|
Pulse Output |
Pulse Constant |
|
Set the pulses per kWh for the pulse output. |
|
Pulse Width |
|
Set the pulse width (ON time). |
|
|
Overload Alarm |
Alarm |
|
Select whether or not the Overload Alarm is enabled:
|
|
Active L setpoint |
Active L setpoint |
1 – 9999 |
Specifies the minimum average current at the load before the timer starts. The meter begins counting the number of seconds the load timer is on (i.e., whenever the readings are equal to or above this average current threshold). |
|
Contrast |
Contrast |
1 – 9 |
Increase or decrease the value to increase or decrease the display contrast. |
|
Reset Config |
Reset Config |
— |
Settings are reset to their defaults. |
|
Exit Config |
Exit Config |
— |
Return to the meter’s main page. |