Set Date/Time
| Command Number | Action | Size | Type | Unit | Range | Description | 
|---|---|---|---|---|---|---|
| 1003 | W | 1 | UInt16 | — | — | (Reserved) | 
| W | 1 | UInt16 | — | 2000 – 2099 | Year | |
| W | 1 | UInt16 | — | 1 – 12 | Month | |
| W | 1 | UInt16 | — | 1 – 31 | Day | |
| W | 1 | UInt16 | — | 0 – 23 | Hour | |
| W | 1 | UInt16 | — | 0 – 59 | Minute | |
| W | 1 | UInt16 | — | 0 – 59 | Second | |
| W | 1 | UInt16 | — | — | (Reserved) |