7EN02-0495-01

Meter overview: EM3200 series

 

A

Pulse output (EM3212)

EM3212

EM3224

EM3212 / EM3224

 

B

Modbus communication port (EM3224)

 

C

Modbus communication LED (EM3224)

 

D

Display with white backlight for measurement and configuration

 

E

Scroll through screens or a list of options

 

F

Confirm entry or access more screens

 

G

Cancel and go back to previous screen

 

H

L1, L2, L3, N

 

I

Energy pulse LED

 

J

Status LED: on / off / error

 

K

Sealing points (3)

 

L

Sealable covers (2)

 

NOTE: The sealable covers must be installed and sealed to the sealing points with the steel cable. Use steel cable with 1.6 mm (1/16 in) diameter and 152.4 mm (6 in) adjustable length for sealing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?