7EN02-0495-01

Pulse output

Pulse output: EM3212 / EM3412 / EM3712

The pulse output indicates the primary consumption with consideration of transformer ratios.

It can be directly connected to a 24 V DC (< 30 V DC) input on a Zelio or Twido PLC.

For other concentrators, if V DC / Rin > 15 mA, add a resistor Radd = (V DC / 0.01) - Rin Ω

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?