Read Device Identification
|
Object ID |
Name / Description |
Length |
Value |
Note |
|---|---|---|---|---|
|
0x00 |
Vendor Name |
20 |
Schneider Electric |
— |
|
0x01 |
Product Code |
20 |
Commercial reference |
The ProductCode value is identical to the catalog number of each device
|
|
0x02 |
Firmware Revision |
06 |
XXX.YYY.ZZZ |
— |
|
0x03 |
Vendor URL |
20 |
— |
|
|
0x04 |
Product Range |
20 |
EM3000 |
— |
|
0x05 |
Product Model |
20 |
Product Model |
Ex: METSEEM3122 |
|
0x06 |
User Application Name |
20 |
User configurable |
Default = Product model |
The Read Device ID codes 01, 02 and 04 are supported:
-
01 = request to get basic device identification (stream access)
-
02 = request to get regular device identification (stream access)
-
04 = request to get one specific identification object (individual access)
The Modbus request and response are compliant with the Modbus Application Protocol Specification.