Diagnostic codes
| Diagnostic code * | Description | Possible solution | 
|---|---|---|
| — | LCD display is not visible. | Check and adjust LCD contrast. | 
| — | Push buttons do not respond. | Restart the meter by powering off and powering on again. | 
| 101 | Metering stops due to an EEPROM error. Press OK to display total energy consumption. | Enter configuration mode and select Reset Config. | 
| 102 | Metering stops due to a lack of a calibration table. Press OK to display total energy consumption. | Enter configuration mode and select Reset Config. | 
| 201 | Metering continues. Mismatch between frequency settings and frequency measurements. | Correct the frequency settings according to the nominal frequency of the power system. | 
| 202 | Metering continues. Mismatch between wiring settings and wiring inputs. | Correct the wiring settings according to wiring inputs. | 
| 203 | Metering continues. Phase sequence reversed. | Check the wire connections and correct the wiring settings if needed. | 
| 204 | Metering continues. Total active energy is negative due to incorrect voltage and current connections. | Check the wire connections and correct the wiring settings if needed. | 
| 205 | Metering continues. Date and Time have been reset due to a loss of power. | Set the Date and Time. | 
| 206 | Metering continues. Pulse is missing due to overload on energy pulse output. | Check the energy pulse output settings and correct if needed. | 
| 207 | Metering continues. Abnormal internal clock function. | Restart the meter by powering off and powering on again then reset the date and time. |