7EN02-0495-01

Meter overview: EM3300 series

EM3322

EM3322

 

A

Modbus communication port

 

B

Modbus communication LED

 

C

Display with white backlight for measurement and configuration

 

D

Scroll through screens or a list of options

 

E

Confirm entry or access more screens

 

F

Cancel and go back to previous screen

 

G

L1, L2, L3, N

 

H

Energy pulse LED

 

I

Status LED: on / off / error

 

J

Sealing points (4)

 

K

Sealable covers (2)

 

NOTE: The sealable covers must be installed and sealed to the sealing points with the steel cable. Use steel cable with 1.6 mm (1/16 in) diameter and 152.4 mm (6 in) adjustable length for sealing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?