7EN02-0495-01

Function list

The table below lists the supported Modbus functions:

Function code

Function name

Decimal

Hexadecimal

3

0x03

Read Holding Registers

16

0x10

Write Multiple Registers

43/14

0x2B/0x0E

Read Device Identification

For example:

  • To read different parameters from the meter, use function 3 (Read).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?