Configuration menu for EM3724
|
Section |
Parameter |
Options |
Description |
|---|---|---|---|
|
Wiring |
Type |
|
Select the power system type the meter is wired to. |
|
VT |
|
Select how many voltage transformers (VT) are connected to the electrical power system. |
|
|
CT |
|
Define how many current transformers (CT) are connected to the meter and which terminals they are connected to. |
|
|
CT & VT Ratio |
CT Secondary |
|
Select the size of the CT secondary, in Amps. |
|
CT Primary |
1 to 32767 |
Enter the size of the CT primary, in Amps. |
|
|
VT Secondary |
|
Select the size of the VT secondary, in Volts. |
|
|
VT Primary |
1 to 1000000 |
Enter the size of the VT primary, in Volts. |
|
|
Frequency |
Frequency |
|
Select the frequency of the electrical power system, in Hz. |
|
Date |
Date |
DD-MMM-YYYY |
Set the current date using the specified format. |
|
Time |
Time |
hh:mm |
Set the time using the 24-hour format. |
|
Communication |
Slave Address |
1 – 247 |
Set the address for this device. The address must be unique for each device in a communications loop. |
|
Baud Rate |
|
Select the speed for data transmission. The baud rate must be the same for all devices in a communications loop. |
|
|
Parity |
|
Select None if the parity bit is not used. The parity setting must be the same for all devices in a communications loop.
NOTE: Number of stop bits = 1 and 2
|
|
|
Com.Protection |
Com.Protection |
|
Protects selected settings and resets from configuration using communications. |
|
Overload Alarm |
Alarm |
|
Select whether or not the Overload Alarm is enabled:
|
|
Active L setpoint |
Active L setpoint |
— |
Specifies the minimum average current at the load before the timer starts. The meter begins counting the number of seconds the load timer is on (i.e., whenever the readings are equal to or above this average current threshold). |
|
Contrast |
Contrast |
1 – 9 |
Increase or decrease the value to increase or decrease the display contrast. |
|
Password |
Password |
0 – 9999 |
Sets the password for accessing the meter configuration screens and resets. |
|
Reset Config |
Reset Config |
— |
Settings are reset to their defaults. |
|
Exit Config |
Exit Config |
— |
Return to the meter’s main page. |