DOCA0355EN-01

Device Internal Error Logs

Description

The last 20 device internal errors are recorded by the LTMT main unit. Each detected internal error log is composed of 8 registers.

A read request of 8xn registers is necessary to read n detected internal error logs, where 8 is the number of registers for each detected internal error log.

The order and the description of the registers for detected internal error log 1 are valid for the other detected internal error logs.

Address Register Description
0x1F40–0x1F47 8001–8008

Detected internal error log 1 (most recent log)

... ... ...
0x1F40–0x1F47 8001+8x(n-1) – 8008+8x(n-1) Detected internal error log n
... ... ...
0x1FD8–0x1FDF 8153–8160 Detected internal error log 20

Device Internal Error Log 1 Registers

The table lists the registers for the detected internal error log 1.

Address

Register

No.

Function code

RW

X

Unit

Type

Svd

Description

0x1F40 8001 4

0x03

R

UINT16

Y

Date and Time

0x1F44 8005 1

0x03

R

UINT16

Y Detected Internal Error Code
0x1F45 8006 3

0x03

R

UINT16

Y Reserved
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.