DOCA0355EN-01

Voltage Dip

The table lists the voltage dip for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EAD

3758

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Load shedding
  • 2: Auto restart

0

Y

Function setting

0x0EAE

3759

1

0x03,
0x06,
0x10

RW

1

%Vn

UINT16

20–90
(step 5)

90

Y

Voltage dip

0x0EAF

3760

1

0x03,
0x06,
0x10

RW

1

%Vn

UINT16

20–95
(step 5)

95

Y

Voltage restoration

0x0EB0

3761

1

0x03,
0x06,
0x10

RW

1

s

UINT16

0–9999
(step 1)

2

Y

Voltage dip restart timeout

0x0EB1

3762

1

0x03,
0x06,
0x10

RW

1

s

UINT16

0–301
(step 1)

4

Y

Delayed restart timeout

0x0EB2

3763

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Bypass STOP DI

0x0EB3

3764

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–4
(step 1)

2

Y

Immediate restart timeout

0x0EB4

3765

1

0x03,
0x06,
0x10

RW

1

s

UINT16

1–9999
(step 1)

10

Y

Load shedding timeout

0x0EB5

3766

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.