DOCA0355EN-01

Motor Data

The table lists the motor data for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Svd

Description

0x15B5

5558

1

0x03

R

1

UINT16

N

Motor status

  • 1: Stop

  • 2: Start

  • 4: Run

0x15B6

5559

1

0x03

R

1

%

UINT16

Y

Thermal memory

0x15B7

5560

2

0x03

R

1

s

UINT32

N

Thermal time to trip

0x15B9

5562

2

0x03

R

1

s

UINT32

N

Thermal time to cool

0x15BB

5564

1

0x03

R

1

UINT16

Y

Max starts counter or Max starts per hour counter

0x15BC

5565

2

0x03

R

1

s

UINT32

Y

Max start time or Max start inhibit time

0x15BE

5567

2

0x03

R

0.001

A

UINT32

N

Motor starting peak current

0x15C0

5569

2

0x03

R

0.001

s

UINT32

N

Motor starting time

0x15C2

5571

2

0x03

R

1

min

UINT32

Y

Total run hour

0x15C4

5573

2

0x03

R

1

min

UINT32

Y

Last run hour

0x15C6

5575

1

0x03

R

1

UINT16

Y

Number of starts

0x15C7

5576

1

0x03

R

1

UINT16

Y

Number of stops

0x15C8

5577

1

0x03

R

1

UINT16

Y

Motor stop cause

  • 0: None

  • 1: HMI

    /DTM
  • 2: Local DI

  • 3: Remote DI

  • 4: Communication

  • 5: Voltage dip

  • 6: Trip

  • 7: No Current

  • 8: Forced stop

  • 9: Direction change

  • 10: No feedback

  • 11: Speed change

  • 12: Custom command

  • 13: Mode transfer

  • 14: Fall-back mode

  • 15: No voltage

0x15C9

5578

1

0x03

R

1

UINT16

Y

Trip counter

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.