DOCA0355EN-01

Maximum Number of Starts

The table lists the maximum number of starts for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EB6

3767

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

1

Y

Function setting

0x0EB7

3768

1

0x03,
0x06,
0x10

RW

1

UINT16

1–30
(step 1)

6

Y

Permissive starts

0x0EB8

3769

1

0x03,
0x06,
0x10

RW

1

min

UINT16

15–60
(step 1)

30

Y

Reference time

0x0EB9

3770

1

0x03,
0x06,
0x10

RW

1

min

UINT16

1–120
(step 1)

5

Y

Inhibit period

0x0EBA

3771

1

0x03,
0x06,
0x10

RW

1

min

UINT16

0–120
(step 1)

0

Y

Time between starts

0x0EBB

3772

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.