DOCA0355EN-01

Event Logs

Description

The last 100 events are recorded by the LTMT main unit. Each event log is composed of 8 registers.

A read request of 8xn registers is necessary to read n event logs, where 8 is the number of registers for each event log.

The order and the description of the registers for event log 1 are valid for the other event logs.

Address Register Description
0x1B58–0x1B5F 7001–7008 Event log 1 (most recent log)
... ... ...
0x1858–0x1B57 7001+8x(n-1) – 7008+8x(n-1) Event log n
... ... ...
0x1E70–0x1E77 7793–7800 Event log 100

Event Log 1 Registers

The table lists the registers for the event log 1.

Address

Register

No.

Function code

RW

X

Unit

Type

Svd

Description

0x1B58 7001 4

0x03

R

UINT16

Y

Date and Time

0x1B5C 7005 1

0x03

R

UINT16

Y Event Code
0x1B5D 7006 3

0x03

R

UINT16

Y Reserved
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.