DOCA0355EN-01

Calculated Ground Trip

The table lists the calculated ground trip for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DE0

3553

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

2

Y

Function setting

0x0DE1

3554

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

10–500
(step 1)

20

Y

Pickup

0x0DE2

3555

1

0x03,
0x06,
0x10

RW

0.010–10

s

UINT16

5–60000
(step 1)

20

Y

Time delay

0x0DE3

3556

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

10–500
(step 1)

20

Y

Alarm level

0x0DE4

3557

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0DE5

3558

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0DE6

3559

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

N

Function while motor starting

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.