DOCA0355EN-01

Normal Inverse Overcurrent Protection

The table lists the normal inverse overcurrent protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DD2

3539

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm + Trip

0

Y

Function setting

0x0DD3

3540

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

20–1000
(step 1)

50

Y

Pickup

0x0DD4

3541

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–200
(step 1)

1

Y

Time multiplier (TMS)

0x0DD5

3542

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

20–1000
(step 1)

50

Y

Alarm level

0x0DD6

3543

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0DD7

3544

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0DD8

3545

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.