DOCA0355EN-01

Block Output

The table lists the block output for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0ED6

3799

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

0x0ED7

3800

1

0x03,
0x06,
0x10

RW

0.01

s

UINT16

0–60000
(step 1)

0

Y

Contactor or Breaker open time

0x0ED8

3801

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.