DOCA0355EN-01

Manufacturing Data

The table lists the manufacturing data for the Modbus RTU communication.

Address

Register

No.

Function code

RW

Type

Svd

Description

0x23A5

9126

2

0x03

R

UINT32

Y

Product Id

0x23A7

9128

16

0x03

R

ASCII

Y

Product serial number

0x23B7

9144

1

0x03

R

UINT16

Y

Manufacture day

0x23B8

9145

1

0x03

R

UINT16

Y

Manufacture month

0x23B9

9146

1

0x03

R

UINT16

Y

Manufacture year

0x23BA

9147

1

0x03

R

UINT16

Y

Manufacture hour

0x23BB

9148

1

0x03

R

UINT16

Y

Manufacture minute

0x23BC

9149

1

0x03

R

UINT16

Y

Manufacture second

0x23BD

9150

2

0x03

R

UINT16

Y

Standard package version

0x23BF

9152

1

Reserved

0x23C0

9153

10

0x03

R

ASCII

Y

Commercial reference

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.