DOCA0355EN-01

Analog Input Protection Settings

Description

The TeSys Tera system supports up to four analog inputs with two LTMTAN21 expansion units.

Each analog input protection settings are made up of eight registers. The order and the description of the settings for analog input 1 are valid for the other analog inputs.

Address

Register

RW

Function code

Description

0x0FA0–0x0FA7

4001–4008

RW

0x03,0x06,0x10

Analog input 1 protection settings

0x0FA8–0x0FAF

4009–4016

RW

0x03,0x06,0x10

Analog input 2 protection settings

0x0FB0–0x0FB7

4017-4024

RW

0x03,0x06,0x10

Analog input 3 protection settings

0x0FB8–0x0FBF

4025–4032

RW

0x03,0x06,0x10

Analog input 4 protection settings

Analog Input 1 Protection Settings

The table lists the registers for the analog input protection settings.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0FA0

4001

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

0

Y

Function setting

0x0FA1

4002

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Under

  • 1: Over

0

Y

Detection

0x0FA2

4003

1

0x03,
0x06,
0x10

RW

0.1

mA

UINT16

40–200
(step 1)

40

Y

Pickup

0x0FA3

4004

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Time delay

0x0FA4

4005

1

0x03,
0x06,
0x10

RW

0.1

mA

UINT16

40–200
(step 1)

40

Y

Alarm

0x0FA5

4006

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0FA6

4007

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0FA7

4008

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.