DOCA0355EN-01

Last Motor Start Time Stamp

The table lists the last motor start time stamp for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Svd

Description

0x15CA

5579

1

0x03

R

1

0

UINT16

Y

Day

0x15CB

5580

1

0x03

R

1

0

UINT16

Y

Month

0x15CC

5581

1

0x03

R

1

0

UINT16

Y

Year

0x15CD

5582

1

0x03

R

1

h

UINT16

Y

Hour

0x15CE

5583

1

0x03

R

1

min

UINT16

Y

Minute

0x15CF

5584

1

0x03

R

1

s

UINT16

Y

Second

0x15D0

5585

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.