DOCA0355EN-01

Statistic Data

The table lists the statistic data for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Svd

Description

0x1676

5751

1

0x03

R

1

ms

UINT16

N

Timer 1 - Actual value

0x1677

5752

1

0x03

R

1

ms

UINT16

N

Timer 2 - Actual value

0x1678

5753

1

0x03

R

1

ms

UINT16

N

Timer 3 - Actual value

0x1679

5754

1

0x03

R

1

ms

UINT16

N

Timer 4 - Actual value

0x167A

5755

1

0x03

R

1

UINT16

N

Counter 1 - Actual value

0x167B

5756

1

0x03

R

1

UINT16

N

Counter 2 - Actual value

0x167C

5757

1

0x03

R

1

UINT16

N

Counter 3 - Actual value

0x167D

5758

1

0x03

R

1

UINT16

N

Counter 4 - Actual value

0x167E

5759

1

0x03

R

1

UINT16

N

Thermal overload trip counter

0x167F

5760

1

0x03

R

1

UINT16

N

Locked rotor trip counter

0x1680

5761

1

0x03

R

1

UINT16

N

Stalled rotor trip counter

0x1681

5762

1

0x03

R

1

UINT16

N

Definite time overcurrent trip counter

0x1682

5763

1

0x03

R

1

UINT16

N

Normal inverse overcurrent trip counter

0x1683

5764

1

0x03

R

1

UINT16

N

Short time overcurrent trip counter

0x1684

5765

1

0x03

R

1

UINT16

N

Calculated ground trip counter

0x1685

5766

1

0x03

R

1

UINT16

N

Measured ground trip counter

0x1686

5767

1

0x03

R

1

UINT16

N

Phase under current trip counter

0x1687

5768

1

0x03

R

1

UINT16

N

Current imbalance trip counter

0x1688

5769

1

0x03

R

1

UINT16

N

Current phase loss trip counter

0x1689

5770

1

0x03

R

1

UINT16

N

Current phase reversal trip counter

0x168A

5771

1

0x03

R

1

UINT16

N

Phase under voltage trip counter

0x168B

5772

1

0x03

R

1

UINT16

N

Phase over voltage trip counter

0x168C

5773

1

0x03

R

1

UINT16

N

Voltage phase loss trip counter

0x168D

5774

1

0x03

R

1

UINT16

N

Voltage imbalance trip counter

0x168E

5775

1

0x03

R

1

UINT16

N

Voltage phase reversal trip counter

0x168F

5776

1

0x03

R

1

UINT16

N

Under frequency trip counter

0x1690

5777

1

0x03

R

1

UINT16

N

Over frequency trip counter

0x1691

5778

1

0x03

R

1

UINT16

N

Excessive start time trip counter

0x1692

5779

1

0x03

R

1

UINT16

N

Communication loss trip counter

0x1693

5780

1

0x03

R

1

UINT16

N

LTMT main unit temperature trip counter

0x1694

5781

1

0x03

R

1

UINT16

N

Under power trip counter

0x1695

5782

1

0x03

R

1

UINT16

N

Over power trip counter

0x1696

5783

1

0x03

R

1

UINT16

N

Under power factor trip counter

0x1697

5784

1

Reserved

0x1698

5785

1

0x03

R

1

UINT16

N

Device internal trip counter

0x1699

5786

1

0x03

R

1

UINT16

N

HMI communication loss trip counter

0x169A–0x169D

5787 – 5790

1

Reserved

0x169E

5791

1

0x03

R

1

UINT16

N

DI interlock 1 trip counter

0x169F

5792

1

0x03

R

1

UINT16

N

DI interlock 2 trip counter

0x16A0

5793

1

0x03

R

1

UINT16

N

DI interlock 3 trip counter

0x16A1

5794

1

0x03

R

1

UINT16

N

DI interlock 4 trip counter

0x16A2

5795

1

0x03

R

1

UINT16

N

DI interlock 5 trip counter

0x16A3

5796

1

0x03

R

1

UINT16

N

DI interlock 6 trip counter

0x16A4

5797

1

0x03

R

1

UINT16

N

DI interlock 7 trip counter

0x16A5

5798

1

0x03

R

1

UINT16

N

DI interlock 8 trip counter

0x16A6

5799

1

0x03

R

1

UINT16

N

DI interlock 9 trip counter

0x16A7

5800

1

0x03

R

1

UINT16

N

DI interlock 10 trip counter

0x16A8

5801

1

0x03

R

1

UINT16

N

DI interlock 11 trip counter

0x16A9

5802

1

0x03

R

1

UINT16

N

DI interlock 12 trip counter

0x16AA

5803

1

Reserved

0x16AF–0x16C1

5807–5822

1

Reserved

0x16BE

5823

1

0x03

R

1

UINT16

N

Analog input 1 trip counter

0x16BF

5824

1

0x03

R

1

UINT16

N

Analog input 2 trip counter

0x16C0

5825

1

0x03

R

1

UINT16

N

Analog input 3 trip counter

0x16C1

5826

1

0x03

R

1

UINT16

N

Analog input 4 trip counter

0x16C2

5827

1

0x03

R

1

UINT16

N

Analog 1 output

@Updated D5

0x16C3

5828

1

0x03

R

1

UINT16

N

Analog 2 output

@Updated D5

0x16C4

5829

1

0x03

R

1

UINT16

N

Motor stop error detection trip counter

0x16C5

5830

1

0x03

R

1

UINT16

N

Logic test interrupted trip counter

0x16C6

5831

1

0x03

R

1

UINT16

N

Stucked reset key trip counter

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.