DOCA0355EN-01

Over Frequency Protection

The table lists the over frequency protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E50

3665

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

0

Y

Function setting

0x0E51

3666

1

0x03,
0x06,
0x10

RW

1

%F*

UINT16

100–110
(step 1)

105

Y

Pickup

0x0E52

3667

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

0x0E53

3668

1

0x03,
0x06,
0x10

RW

1

%F*

UINT16

100–110
(step 1)

105

Y

Alarm level

0x0E54

3669

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset Key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E55

3670

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E56

3671

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.