DOCA0355EN-01

BITMAP Representation of Boolean Data

The boolean data can also be mapped using bitwise data. For example, the Digital Input Status is mapped bitwise in the following table.

BITMAP register

BITMAP function code

Boolean register

Boolean function code

Description

5627.0

0x03

1

0x02

Digital Input 1

5627.1

0x03

2

0x02

Digital Input 2

5627.2

0x03

3

0x02

Digital Input 3

5627.3

0x03

4

0x02

Digital Input 4

5627.4

0x03

5

0x02

Digital Input 5

5627.5

0x03

6

0x02

Digital Input 6

5627.6

0x03

7

0x02

Digital Input 7

5627.7

0x03

8

0x02

Digital Input 8

5627.8

0x03

9

0x02

Digital Input 9

5627.9

0x03

10

0x02

Digital Input 10

5627.10

0x03

11

0x02

Digital Input 11

5627.11

0x03

12

0x02

Digital Input 12

5627.12

0x03

13

0x02

Digital Input 13

5627.13

0x03

14

0x02

Digital Input 14

5627.14

0x03

15

0x02

Digital Input 15

5627.15

0x03

16

0x02

Digital Input 16

5626.0

0x03

17

0x02

Digital Input 17

5626.1

0x03

18

0x02

Digital Input 18

5626.2

0x03

19

0x02

Digital Input 19

5626.3

0x03

20

0x02

Digital Input 20

5626.4

0x03

21

0x02

Digital Input 21

5626.5

0x03

22

0x02

Digital Input 22

5626.6

0x03

23

0x02

Digital Input 23

5626.7

0x03

24

0x02

Digital Input 24

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.