DOCA0355EN-01

Modbus RTU HMI Connection Port

The HMI port on LTMT main unit with Modbus RTU protocol can also be used as an optional Modbus RTU communication port.

When the LTMT HMI port is used as Modbus RTU communication port:

  • LTMT main unit is connected to a Modbus RTU client in a point-to-point connection.

  • Modbus RTU client can be connected to the HMI port.

  • HMI port can be connected temporarily to a PC running the TeSys Tera DTM embedded in a FDT container for TeSys Tera system configuration.

The HMI port characteristics are:

Physical interface RS 485 wire
Connector RJ45

Connection Diagram

A Modbus RTU client can be connected to the HMI port on the front face of the LTMT main unit, as shown in the diagram below.

A Modbus RTU client (PC or PLC)
B Modbus RTU cable
C LTMT main unit

Modbus RTU Cables

The table lists the Modbus RTU cables used for connection.

Designation

Length

Shielded cable for Modbus RTU bus, with two RJ45 connectors

0.3 m (1 ft)

1 m (3.2 ft)

3 m (9.8 ft)

Connection cable USB or RJ45 2.5 m (8.20 ft)

LTMT HMI Port Pinout

The LTMT main unit is connected to the Modbus RTU network with a shielded RJ45 connector in compliance with the following wiring:

Pin No.

Signal

Description

1

Not connected

2

Not connected

3

Not connected

4

D1 or D(B)

Transceiver terminal 1

5

D0 or D(A)

Transceiver terminal 0

6

Not connected

7

+5V

Auxiliary supply to HMI

8

0VL

Signal and power supply common

LTMT HMI Port Settings

The LTMT HMI port has the following configurable settings:

Setting Setting range Default setting
Node address 1–247 in step of 1 1
Parity
  • None

  • Odd

  • Even

Even

Baud rate
  • 2400 bps

  • 4800 bps

  • 9600 bps

  • 19200 bps

  • 38400 bps

  • 57600 bps

  • 115200 bps

19200 bps

Endianness

  • Big-endian

  • Little-endian

Big-endian

NOTE: If LTMTCUF control operator unit is connected on HMI port, then HMI port must be configured as follows:
  • Node address: 1

  • Baud rate: 19200 bps

  • Parity: Even

  • Endianness: Big-endian

The LTMT HMI port settings can be configured using the following interfaces:

  • A PC running the TeSys Tera DTM embedded in a FDT container, such as SoMove software.

  • A PLC or DCS through the communication protocol.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.