DOCA0355EN-01

Function Codes

The TeSys Tera system supports the following Modbus RTU function codes:

Function Code

Description

2 (0x02)

Read discrete inputs

3 (0x03)

Read holding registers

4 (0x04)

Read input registers

6 (0x06)

Write single holding register

16 (0x10)

Write multiple holding registers

23 (0x17)

Read or Write multiple holding registers

43 or 14 (0x2B or 0x0E)

Read device identification

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.