DOCA0355EN-01

LTMTCT/LTMTCTV Sensor Module Device Internal Error Detection

The table lists the different device internal error detection setting for the LTMTCT/LTMTCTV sensor module Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0280

641

0x02

R

BOOL N

Watchdog timeout detected

0x0281

642

0x02

R

BOOL N

ADC conversion error detected

0x0282

643

0x02

R

BOOL N

Flash error detected

0x0283

644

Reserved

0x0284

645

0x02

R

BOOL N

Voltage configuration not detected

0x0285

646

Reserved

0x0286

647

0x02

R

BOOL N

Calibration error detected

0x0287

648

0x02

R

BOOL N

VL1 measurement error detected

0x0288

649

0x02

R

BOOL N

VL2 measurement error detected

0x0289

650

0x02

R

BOOL N

VL3 measurement error detected

0x028A

651

0x02

R

BOOL N

IL1 low gain measurement error detected

0x028B

652

0x02

R

BOOL N

IL1 high gain measurement error detected

0x028C

653

0x02

R

BOOL N

IL2 low gain measurement error detected

0x028D

654

0x02

R

BOOL N

IL2 high gain measurement error detected

0x028E

655

0x02

R

BOOL N

IL3 low gain measurement error detected

0x028F

656

0x02

R

BOOL N

IL3 high gain measurement error detected

0x0290–0x029F

657–672

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.