DOCA0355EN-01

Analog Comparator Output Status

The table lists the analog comparator output status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x00C0

193

0x02

R

BOOL N

Analog comparator output 1

0x00C1

194

0x02

R

BOOL N

Analog comparator output 2

0x00C2

195

0x02

R

BOOL N

Analog comparator output 3

0x00C3

196

0x02

R

BOOL N

Analog comparator output 4

0x00C4–0x00CF

197–208

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.