DOCA0355EN-01

Stalled Rotor Protection

The table lists the stalled rotor protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DBE

3519

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

2

Y

Function

setting

0x0DBF

3520

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

50–1000
(step 1)

200

Y

Pickup 

0x0DC0

3521

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

20

Y

Time delay

0x0DC1

3522

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

50–1000
(step 1)

200

Y

Alarm level

0x0DC2

3523

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

0x0DC3

3524

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset Delay

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.