DOCA0355EN-01

Under Power Protection

The table lists the under power protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E57

3672

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

0

Y

Function setting

0x0E58

3673

1

0x03,
0x06,
0x10

RW

1

%P

%P = % of nominal power.

The nominal power (Pn) is calculated by the LTMT main unit from the system settings: Pn = VT primary * Full load current.

In case of two-speed motor starters, the nominal power is:

  • Pn1 = VT primary * Full load current, when the motor runs in speed 1 or low speed

  • Pn2 = VT primary * Speed 2 Full load current, when the motor runs in speed 2 or high speed

*

UINT16

20–1000
(step 1)

60

Y

Pickup

0x0E59

3674

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

0x0E5A

3675

1

0x03,
0x06,
0x10

RW

1

%P

%P = % of nominal power.

The nominal power (Pn) is calculated by the LTMT main unit from the system settings: Pn = VT primary * Full load current.

In case of two-speed motor starters, the nominal power is:

  • Pn1 = VT primary * Full load current, when the motor runs in speed 1 or low speed

  • Pn2 = VT primary * Speed 2 Full load current, when the motor runs in speed 2 or high speed

*

UINT16

20–1000
(step 1)

60

Y

Alarm level

0x0E5B

3676

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset Key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E5C

3677

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E5D

3678

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.