DOCA0355EN-01

Hysteresis Settings

The table lists the registers for the hysteresis settings.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x109A

4251

1

0x03,
0x06,
0x10

RW

1

%

UINT16

3–15
(step 1)

3

Y

Current protection

0x109B

4252

1

0x03,
0x06,
0x10

RW

1

%

UINT16

3–15
(step 1)

3

Y

Voltage protection

0x109C

4253

1

0x03,
0x06,
0x10

RW

1

%

UINT16

1–15
(step 1)

3

Y

Frequency protection

0x109D

4254

1

0x03,
0x06,
0x10

RW

1

%

UINT16

3–15
(step 1)

3

Y

Power protection

0x109E

4255

1

0x03,
0x06,
0x10

RW

1

mA

UINT16

1–3
(step 1)

1

Y

Analog input protection

0x109E–0x109F

4256

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.