DOCA0355EN-01

HMI Communication Loss

The table lists the HMI communication loss for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EDE

3807

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm+Trip

0

Y

Function setting

0x0EDF

3808

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

10

Y

Time delay

0x0EE0

3809

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

0x0EE1

3810

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0

Y

Auto-Reset delay

0x0EE2

3811

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.