DOCA0355EN-01

User Map Data for Registers

The user map data are designed to optimize the access to 100 non-continuous registers maximum in one single request.

You can define several read and write areas.

The user map can be defined via:

  • PC running the TeSys Tera DTM Library embedded in a FDT container like SoMove software.

  • PLC or DCS through the communication network.

User Map Addresses

The user map addresses are used to select a list of addresses to read or write. It can be considered as a configuration area.

Address

Register

No.

Function code

RW

Type

Range

Svd

Description

0x0320

801

1

0x03,
0x06,
0x10

RW

UINT16

1-9249

Y

User map address 1

0x0321

802

1

0x03,
0x06,
0x10

RW

UINT16

1-9249

Y

User map address 2

0x0322

803

1

0x03,
0x06,
0x10

RW

UINT16

1-9249

Y

User map address 3

0x0383

900

1

0x03,
0x06,
0x10

RW

UINT16

1-9249

Y

User map address 100

User Map Values

The user map values are used to read or write values associated to addresses configured in the user map addresses.

Address

Register

No.

Function code

RW

Type

Range

Svd

Description

0x0384

901

1

0x03,
0x06,
0x10

RW

UINT16

1-65535

N

User map value 1

0x0385

902

1

0x03,
0x06,
0x10

RW

UINT16

1-65535

N

User map value 2

0x0386

903

1

0x03,
0x06,
0x10

RW

UINT16

1-65535

N

User map value 3

0x03E7

1000

1

0x03,
0x06,
0x10

RW

UINT16

1-65535

N

User map value 100

Read or write of address 0x0384 or register 901 allows to read or write the value in address defined in address 0x0320 or register 801.

Read or write of address 0x0385 or register 902 allows to read or write the value in address defined in address 0x0321 or register 802, and so on.

Examples

The following table gives an example of user map address configuration to access non-continuous registers:

Address

Register

Register Value (user map address to be configured)

Description of user map address

0x0320

801

0x15B5

Motor status

0x0321

802

0x15C8

Motor stop cause

0x0322

803

0x160D

Trip status MSW

0x0323

804

0x160E

Trip status LSW

0x0324

805

0x15B6

Thermal memory

0x0325

806

0x1586

Average current (0.001 A) MSW

0x0326

807

0x1587

Average current (0.001 A) LSW

0x0352

851

0x02C0

Control register 1

0x0353

852

0x02C1

Control register 2

With this configuration, monitoring information is accessible with one single read request through addresses 0x0384 to 0x038A or registers 901 to 907.

Configuration and command can be written with one single write using addresses 0x03B6 to 0x03B7 or registers 951 to 952.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.