DOCA0355EN-01

Locked Rotor Protection

The table lists the locked rotor protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DC4

3525

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

2

Y

Function setting

0x0DC5

3526

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

150–1000
(step 1)

200

Y

Pickup

0x0DC6

3527

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

100

Y

Time delay

0x0DC7

3528

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

150–1000
(step 1)

200

Y

Alarm level

0x0DC8

3529

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

0x0DC9

3530

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto–Reset delay

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.