DOCA0355EN-01

Temperature Protection

The table lists the temperature protection for the LTMT main unit.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0ECD

3790

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

0

Y

Function setting

0x0ECE

3791

1

0x03,
0x06,
0x10

RW

0.1

°C

UINT16

250–1800
(step 1)

1300

Y

PT100 pickup*

F

770-3560
(step 1)

0x0ECF

3792

1

0x03,
0x06,
0x10

RW

1

Ω

UINT16

2700–4000
(step 1)

2700

Y

PTC pickup

0x0ED0

3793

1

0x03,
0x06,
0x10

RW

1

Ω

UINT16

1600–2300
(step 1)

1600

Y

PTC pickup reset

0x0ED1

3794

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

10

Y

Time delay

0x0ED2

3795

1

0x03,
0x06,
0x10

RW

0.1

°C

UINT16

250–1800
(step 1)

1300

Y

PT100 alarm level*

F

770-3560
(step 1)

0x0ED3

3796

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0ED4

3797

1

0x03,
0x06,
0x10

RW

0.1

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0ED5

3798

1

0x03,
0x06,
0x10

RW

0

UINT16

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.