DOCA0355EN-01

LTMT HMI Port Settings

The table lists the HMI port settings for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X Unit

Type

Range Default value

Svd

Description

0x112F

4400

1

0x03,0x10

RW

1

UINT16

1–247
(step 1)

1

Y

Node address

0x1130

4401

1

0x03,0x10

RW

1

UINT16

0: None

1: Odd

2: Even

2

Y

Modbus parity

0x1131

4402

1

0x03,0x10

RW

1 bps

UINT16

0: 2400

1: 4800

2: 9600

3: 19200

4: 38400

5: 57600

6: 115200

3

Y

Baud rate

0x1132

4403

1

0x03,0x10

RW

1

UINT16

0: Default

1: Programmable

N

Control keys

0x1133

4404

1

0x03,0x10

RW

1

s

UINT16

1–6000
(step 1)

1

Y

Timeout

0x1134 4405 1 0x03,0x10 RW BITMAP

0: Big-endian

1: Little-endian

0 Y Byte format

NOTE: If LTMTCUF control operator unit is connected on HMI port, HMI port must be configured as follows:
  • Node address: 1

  • Baud rate: 19200 bps

  • Parity: Even

  • Endianness: Big-endian

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.