DOCA0355EN-01

Communication Status

The table lists the communication status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x02A0

673

0x02

R

BOOL

N

Modbus RTU or PROFIBUS DP port – No communication

0x02A1

674

0x02

R

BOOL

N

HMI port – No communication

0x02A4–0x02BF

677–704

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.