DOCA0355EN-01

Anti-Backspin Timer

The table lists the anti-backspin timer for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EDA

3803

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

0x0EDB

3804

1

0x03,
0x06,
0x10

RW

1

s

UINT16

0–60000
(step 1)

0

Y

Time delay

0x0EDC

3805

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.