DOCA0355EN-01

Analog Protection Status

Analog Protection Alarm Status

The table lists the analog protection alarm status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0190

401

0x02

R

BOOL N

AI1 alarm

0x0191

402

0x02

R

BOOL N

AI2 alarm

0x0192

403

0x02

R

BOOL N

AI3 alarm

0x0193

404

0x02

R

BOOL N

AI4 alarm

0x0194–0x019F

405–416

Reserved

Analog Protection Pickup Status

The table lists the analog protection pickup status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x01A0

417

0x02

R

BOOL N

AI1 pickup

0x01A1

418

0x02

R

BOOL N

AI2 pickup

0x01A2

419

0x02

R

BOOL N

AI3 pickup

0x01A3

420

0x02

R

BOOL N

AI4 pickup

0x01A4–0x01AF

421–432

Reserved

Analog Protection Trip Status

The table lists the analog protection trip status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x01B0

433

0x02

R

BOOL N

AI1 trip

0x01B1

434

0x02

R

BOOL N

AI2 trip

0x01B2

435

0x02

R

BOOL N

AI3 trip

0x01B3

436

0x02

R

BOOL N

AI4 trip

0x01B4–0x01BF

437–448

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.