DOCA0355EN-01

Device Configuration

The table lists the device configuration for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X Unit

Type

Range Default value

Svd

Description

0x1117

4376

1

0x03,
0x06,
0x10

RW

1

UINT16 1–15

8

Y LTMTCT/LTMTCTV Sensor Module Type

0x1118

4377

1

Reserved

0x1119

4378

1

0x03,
0x06,
0x10

RW

1

UINT16 0–8

0

Y LTMT Expansion Unit 1 Type

0x111B

4380

1

0x03,
0x06,
0x10

RW

1

UINT16 0–8

0

Y LTMT Expansion Unit 2 Type

0x111D

4382

1

0x03,
0x06,
0x10

RW

1

UINT16 0–8

0

Y LTMT Expansion Unit 3 Type

0x111F

4384

1

0x03,
0x06,
0x10

RW

1

UINT16 0–8

0

Y LTMT Expansion Unit 4 Type

0x1121

4386

1

0x03,
0x06,
0x10

RW

1

UINT16 0–8

0

Y LTMT Expansion Unit 5 Type

0x1123

4388

1

0x03,
0x06,
0x10

RW

1

UINT16 0–2

0

Y

LTMT main unit temperature sensor type*:

  • 0: None

  • 1: PT100

  • 2: Binary PTC

0x1124

4389–4393

5

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.