DOCA0355EN-01

Overview

This part describes how to connect an LTMT main unit to a RS 485 Modbus RTU network through its 4-terminal connector.

Always follow the recommendations for wiring and connection.

WARNING
LOSS OF CONTROL
  • The designer of any control scheme must consider the potential failure modes of control paths and, for certain critical functions, provide a means to achieve a safe state during and after a path failure. Examples of critical control functions are forced stop and overtravel stop.
  • Separate or redundant control paths must be provided for critical control functions.
  • System control paths may include communication links. Consideration must be given to the implications of anticipated transmission delays or failures of the link.
  • Each implementation of an LTMT main unit must be individually and thoroughly tested for proper operation before being placed into service.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: For additional information, refer to NEMA ICS 1.1 (latest edition), Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.