DOCA0355EN-01

Interlock Protection Status

Interlock Protection Alarm Status

The table lists the interlock protection alarm status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0160

353

0x02

R

BOOL N

Interlock 1 alarm

0x0161

354

0x02

R

BOOL N

Interlock 2 alarm

0x0162

355

0x02

R

BOOL N

Interlock 3 alarm

0x0163

356

0x02

R

BOOL N

Interlock 4 alarm

0x0164

357

0x02

R

BOOL N

Interlock 5 alarm

0x0165

358

0x02

R

BOOL N

Interlock 6 alarm

0x0166

359

0x02

R

BOOL N

Interlock 7 alarm

0x0167

360

0x02

R

BOOL N

Interlock 8 alarm

0x0168

361

0x02

R

BOOL N

Interlock 9 alarm

0x0169

362

0x02

R

BOOL N

Interlock 10 alarm

0x016A

363

0x02

R

BOOL N

Interlock 11 alarm

0x016B

364

0x02

R

BOOL N

Interlock 12 alarm

0x016C–0x016F

365–368

Reserved

Interlock Protection Pickup Status

The table lists the interlock protection pickup status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0170

369

0x02

R

BOOL N

Interlock 1 pickup

0x0171

370

0x02

R

BOOL N

Interlock 2 pickup

0x0172

371

0x02

R

BOOL N

Interlock 3 pickup

0x0173

372

0x02

R

BOOL N

Interlock 4 pickup

0x0174

373

0x02

R

BOOL N

Interlock 5 pickup

0x0175

374

0x02

R

BOOL N

Interlock 6 pickup

0x0176

375

0x02

R

BOOL N

Interlock 7 pickup

0x0177

376

0x02

R

BOOL N

Interlock 8 pickup

0x0178

377

0x02

R

BOOL N

Interlock 9 pickup

0x0179

378

0x02

R

BOOL N

Interlock 10 pickup

0x017A

379

0x02

R

BOOL N

Interlock 11 pickup

0x017B

380

0x02

R

BOOL N

Interlock 12 pickup

0x017C–0x017F

381–384

Reserved

Interlock Protection Trip Status

The table lists the interlock protection trip status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0180

385

0x02

R

BOOL N

Interlock 1 trip

0x0181

386

0x02

R

BOOL N

Interlock 2 trip

0x0182

387

0x02

R

BOOL N

Interlock 3 trip

0x0183

388

0x02

R

BOOL N

Interlock 4 trip

0x0184

389

0x02

R

BOOL N

Interlock 5 trip

0x0185

390

0x02

R

BOOL N

Interlock 6 trip

0x0186

391

0x02

R

BOOL N

Interlock 7 trip

0x0187

392

0x02

R

BOOL N

Interlock 8 trip

0x0188

393

0x02

R

BOOL N

Interlock 9 trip

0x0189

394

0x02

R

BOOL N

Interlock 10 trip

0x018A

395

0x02

R

BOOL N

Interlock 11 trip

0x018B

396

0x02

R

BOOL N

Interlock 12 trip

0x018C–0x018F

397–400

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.