DOCA0355EN-01

Example of Modbus RTU Frames

Request

Request from the client to the LTMT Modbus RTU server at address 5 to read the L1 RMS current, available in a UINT32 register at address 0x157C.

Definition

Number of Bytes

Value

Comment

Server address

1 byte

0x05

TeSys Tera Modbus RTU server address

Function code

1 byte

0x03

Reads n output or internal words

Address

2 bytes

0x157C

Address of the first 16-bit register to read

Number of words

2 bytes

0x0002

Reads 2 16-bit registers

CRC

2 bytes

xyzt

Value of CRC16

Response

Response from the LTMT Modbus RTU server at address 5: L1 RMS current = 87 485 mA.

Definition

Number of Bytes

Value

Comment

Server address

1 byte

0x05

TeSys Tera Modbus RTU server address

Function code

1 byte

0x03

Reads n output or internal words

Number of bytes

1 byte

0x04

Number of bytes to read

Value of words read

4 bytes

0x0001 55BD


(87 485 mA)

Reads 2 registers (L1 RMS curent in mA)

CRC

2 bytes

xyzt

Value of CRC16

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.