DOCA0355EN-01

Phase Under Current Protection

The table lists the phase under current protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DEE

3567

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

1

Y

Function setting

0x0DEF

3568

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

15–100
(step 1)

50

Y

Pickup

0x0DF0

3569

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

100

Y

Time delay

0x0DF1

3570

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

15–100
(step 1)

50

Y

Alarm level

0x0DF2

3571

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

8

Y

Reset mode

0x0DF3

3572

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

50

Y

Auto-Reset delay

0x0DF4

3573

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.