DOCA0355EN-01

Wiring Accessories

Modbus RTU Accessories

The table lists the Modbus RTU accessories used for connection.

Designation

Description

Reference Number

T-junction boxes

Box with two RJ45 socket for trunk cable and an integrated 0.3 m (1 ft) cable with one RJ45 connector for tap-off

Box with two RJ45 socket for trunk cable and an integrated 1 m (3.2 ft) cable with one RJ45 connector for tap-off

Line terminator for RJ45 connector

R = 120 Ω

Line terminator for open-style connector

R = 120 Ω

Modbus RTU Cables

The table lists the Modbus RTU cables used for connection.

Designation

Length

Shielded cable for Modbus RTU bus, with two RJ45 connectors

0.3 m (1 ft)

1 m (3.2 ft)

3 m (9.8 ft)

Shielded cable for Modbus RTU bus, with one RJ45 connectors and one stripped end

3 m (9.8 ft)

Shielded cable for Modbus RTU bus, with two stripped ends

100 m (320 ft)

200 m (640 ft)

500 m (1600 ft)

Belden cable

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.