DOCA0355EN-01

Motor Stop Error Detection

The table lists the motor stop error detection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EBE

3775

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

0x0EBF

3776

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

10

Y

Time delay

0x0EC0

3777

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication

3

Y

Reset mode

0x0EC1

3778

1

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.