DOCA0355EN-01

Digital Output Status

The table lists the digital output status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0020

33

0x02

R

BOOL

N

Digital output 1 

0x0021

34

0x02

R

BOOL

N

Digital output 2

0x0022

35

0x02

R

BOOL

N

Digital output 3

0x0023

36

0x02

R

BOOL

N

Digital output 4

0x0024

37

0x02

R

BOOL

N

Digital output 5

0x0025

38

0x02

R

BOOL

N

Digital output 6

0x0026

39

0x02

R

BOOL

N

Digital output 7

0x0027

40

0x02

R

BOOL

N

Digital output 8

0x0028

41

0x02

R

BOOL

N

Digital output 9

0x0029

42

0x02

R

BOOL

N

Digital output 10

0x002A

43

0x02

R

BOOL

N

Digital output 11

0x002B

44

0x02

R

BOOL

N

Digital output 12

0x002C

45

0x02

R

BOOL

N

Digital output 13

0x002D–0x003F

46–64

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.