Completing SFTP Configuration

Now that you have a hybrid connection, you need to store the SFTP Credential, Public Key, and Target Remote Directory.

  1. In Solution Center in the Client Configuration plugin, click the SFTP Configuration tab.

  2. Populate all fields (the entries in the image below are just examples).

    • All fields are required except for the SFTP Remote File Path. If the Remote File Path is not set, the zipped files are stored in the default working directory as established during your implementation.

    • The SFTP SSH HostKey must be the SHA256 form of the key. It should not contain the algorithm used to encode it.

  3. Click Save.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?