Configuring Tenant to Zip and Upload

With each successfully exported subnetwork, you can have the application upload a zipped Geodatabase Region Resource (GRR) or Group GRR to a predefined SFTP location.

Prerequisites:

Before performing the configuration, you need the following information:

  • Host name of the SFTP server.

  • A username and password to employ for storing files.

  • The Base64 SHA256 public key that was created when you configured the SFTP server.

  • Optionally, the relative path of the remote directory in which you wish to store the zipped GRRs (relative from the initial workspace seen by the user).

Further, you need to download and install the Microsoft Hybrid Connection Manager on the machine that is hosting the SFTP server.


To configure the server in Solution Center:

  1. In Solution Center in the Feeder Services plugin, click the Additional Configuration tab.

  2. Click the Use Zip and Upload to SFTP toggle on.

  3. Click Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?